AXIS#.VL.ARZQ1 TO AXIS#.VL.ARZQ4

Description

AXIS#.VL.ARZQ1 sets the Q (quality factor) of the zero (numerator) of AR filter 1. This value is QZ in the approximate transfer function of the filter:

AR1(s) = [s²/(2πFZ)²+s/(QZ2πFZ) + 1]/ [s²/(2πFP)² +s/(QP2πFP) + 1]

 

The following block diagram describes the AR filter function; note that AR1 and AR2 are in the forward path, while AR3 and AR4 are applied to feedback:

AR1, AR2, AR3 and AR4 are used in velocity and position mode, but are disabled in torque mode.

Discrete time transfer function (applies to all AR filters)

The velocity loop compensation is actually implemented as a digital discrete time system function on the DSP. The continuous time transfer function is converted to the discrete time domain by a backward Euler mapping:

s ≈ (1-z-1)/t, where t = 62.5 µs.

The poles are prewarped to FP and the zeros are prewarped to FZ.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0.1 to 5

Default Value

AXIS#.VL.ARZQ1: 0.707

VLARZQ2 to VLARZQ4: 0.5

Data Type

Float
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
AXIS1.VL.ARZQ1

5011h

1ch

Unsigned32

-

1000:1

Read/Write

No

AXIS1.VL.ARZQ2

5011h

1dh

Unsigned32

-

1000:1

Read/Write

No

AXIS1.VL.ARZQ3

5011h

1eh

Unsigned32

-

1000:1

Read/Write

No

AXIS1.VL.ARZQ4

5011h

1fh

Unsigned32

-

1000:1

Read/Write

No

AXIS2.VL.ARZQ1

5111h

1ch

Unsigned32

-

1000:1

Read/Write

No

AXIS2.VL.ARZQ2

5111h

1dh

Unsigned32

-

1000:1

Read/Write

No

AXIS2.VL.ARZQ3

5111h

1eh

Unsigned32

-

1000:1

Read/Write

No

AXIS2.VL.ARZQ4

5111h

1fh

Unsigned32

-

1000:1

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.VL.ARZQ1

6016

1780

Signed32

Read/Write

-

AXIS2.VL.ARZQ1

71552

1178

Signed32

Read/Write

-

AXIS1.VL.ARZQ2

6017

1781

Signed32

Read/Write

-

AXIS2.VL.ARZQ2

71553

1178

Signed32

Read/Write

-

AXIS1.VL.ARZQ3

6018

1782

Signed32

Read/Write

-

AXIS2.VL.ARZQ3

71554

1178

Signed32

Read/Write

-

AXIS1.VL.ARZQ4

6019

1783

Signed32

Read/Write

-

AXIS2.VL.ARZQ4

71555

1178

Signed32

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.VL.ARZQ1

6016

Float

Read/Write

-

AXIS#.VL.ARZQ2

6017

Float

Read/Write

-

AXIS#.VL.ARZQ3

6018

Float

Read/Write

-

AXIS#.VL.ARZQ4

6019

Float

Read/Write

-